cancel
Showing results for 
Search instead for 
Did you mean: 

MAX485 and STM32 ?

antonius
Senior
Posted on January 01, 2014 at 01:49

Guys,

Can I use MAX485 and STM32F107VCT6?

I can't find VH max on F107 datasheet, is it possible if I interface MAX485 with STM32F107VCT6 USART ? pin PA9 and PA10 connected directly to MAX485

Any clues ?

Thanks

#contact-bounce
4 REPLIES 4
Andrew Neil
Chief II
Posted on January 01, 2014 at 13:51

''I can't find VH max on F107 datasheet''

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1031/LN1564/PF221020

Tables 36-37 ?

antonius
Senior
Posted on January 02, 2014 at 00:10

Found, thank you,

So it's possible if I use 5V supply for MAX485 but the input is from USART1 of STM32F107, do you reckon ?

Any experience on how to use GPIO as input button ?

Posted on January 02, 2014 at 00:59

Both PA9/PA10 are FT (Five Volt Tolerant), an output in OD mode can be pulled to a 5V supply.

Button and GPIO inputs are on practically any Dev/Eval board you can find, look at some schematics.

Typically you have a pull-up to 3V connected to one side of the button, which connects to your GPIO pin, and the other side of the button to ground. With the button not press you see a HIGH, when the button makes to ground you see a LOW.
Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Chief II
Posted on January 02, 2014 at 08:19

Don't forget

http://www.lmgtfy.com?q=contact+bounce

...