cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103VET with SDcard and uClinux ?

antonius
Senior
Posted on April 14, 2014 at 02:41

Guys,

Can I use STM32F103VET6 with SDcard and uClinux?

I put linux on SDcard and use internal RAM or I put linux on NAND flash ?

Do I need external RAM ?

Any ideas on doing that ?

Thanks
2 REPLIES 2
Posted on April 14, 2014 at 05:50

Have you worked with Linux or ucLinux kernels in the past?

With a minimal build of ucLinux how large is it? How large is a build with the feature set you need? What types of boards and memory configuration are people using with ucLinux? Do these seem to correlate with the resources provided by an STM32F103 running at 72 MHz?

http://www.emcraft.com/

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
antonius
Senior
Posted on April 14, 2014 at 08:03

I worked with linux before..