cancel
Showing results for 
Search instead for 
Did you mean: 

How to use STM32CubeF4 ?

antonius
Senior
Posted on April 14, 2015 at 11:46

Hi Guys,

Does anyone know how to use STM32CubeF4 with STM32F4 Discovery board ? Is it similar like using Keil ?

Any clues please ?

Thanks
9 REPLIES 9
l239955_stm1
Associate II
Posted on April 14, 2015 at 13:33

Hi, STM32Cube contains:

- STM32CubeMX - graphical software to design of microcontroller configuration and generating initialization code, it´s very useful for me in order wide application. For Win you can install STM32CubeMX

and under Linux there is Eclipse plugin.

- STM32Cube HAL - it´s new abstraction layer, ensuring portability across STM32 portfolio. Latest microcontrollers are not supported in STM Standard Peripheral Library and you have to use HAL ''library''

antonius
Senior
Posted on April 14, 2015 at 23:44

How can I initialize and use Ethernet (ETH): media access control (MAC) with

DMA controller on STM32F407 Discovery ?

I can't find any examples on STM32F4 Cube and if I want to initialize myself,

I tried following

STM32F4 cube manual, document name : DM00107720.pdf

page 16, am I on the right track ?

Thanks

l239955_stm1
Associate II
Posted on April 15, 2015 at 08:59

I have no experience with stm32f4 and ETH but tool STM32CubeMX generate initialization code for all peripherals that you want to.

There is window in CubeMX with ETH setting

0690X000006052EQAQ.png

antonius
Senior
Posted on April 15, 2015 at 23:32

Where can you find this tool STM32CubeMX?

STM32Cube_FW_F4_V1.5.0\Utilities\ ?

Posted on April 16, 2015 at 02:06

Where can you find this tool STM32CubeMX?

Tried Google?

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF259242?icmp=stm32cubemx_pron_pr-stm32snippets_mar2014&sc=stm32cube-pr1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
antonius
Senior
Amel NASRI
ST Employee
Posted on April 16, 2015 at 15:41

Hi h.rick,

These are some helpful links containing packages to be used besides to required documentation:

- STM32CubeMX: http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242

- STM32CubeF4: http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243

Some Ethernet examples are available in the package STM32CubeF4 under STM32Cube_FW_F4_V1.5.0\Projects\STM324x9I_EVAL\Applications.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

antonius
Senior
Posted on April 17, 2015 at 15:28

Ok,

Thanks for the links...

Is this the application ?

0690X000006030wQAA.jpg

l239955_stm1
Associate II
Posted on April 20, 2015 at 08:22

Yes 🙂