cancel
Showing results for 
Search instead for 
Did you mean: 

Graphic library for LCD to be used with STM32

tecnico23
Associate II
Posted on May 17, 2012 at 15:43

Hi,

I would ask for recommended Graphic Libraries to use with STM32 controlers.

I 've found the ''Resource Editor for Embedded GUI Library'' developed by ST, but there is too few proprieties associated with each object. For example, I can't configure the background, text colour, and resize a button. And you also have few fonts types.

I would like to use a Windows software, where I could built the screens without spend much time. I found emWin developped by Segger. It seems to be good but it is too much expensive for what I really need.

I will need to use:

-Labels;

-Textbox;

-Buttons;

-Sliders;

-Switches;

-Checkboxes;

-Radiobuttons;

-Gauge;

-Picture;

And maybe grahps in the future.

I'm looking for something like ''

eGUI/D4D'' developed by Freescale.

Best regards,

A.Paiva
18 REPLIES 18
emalund
Associate III
Posted on May 17, 2012 at 20:26

something lik this?

http://www.keil.com/forum/20852/

Erik
tecnico23
Associate II
Posted on May 22, 2012 at 11:03

Hi Erik,

I'm not using Keil's IDE.

Thanks for your suggestion,

A. Paiva

oriday
Associate
Posted on May 23, 2012 at 22:35

bjfree
Associate II
Posted on May 24, 2012 at 05:29

I would suggest looking up ardiuno code like:

https://github.com/adafruit/ST7565-LCD

tecnico23
Associate II
Posted on May 25, 2012 at 13:10

Dear BJ Freeman,

Thank you for your suggestion. But I'm looking for a graphical interface where I can see and put the objects in panels, and then the graphical interface should convert the panels into a .c and .h files.

I'm looking for a library like this one developed by ST (''Resource Editor for Embedded GUI Library), but more sophisticated but also low cost.

Thank you very much,

A. Paiva

bjfree
Associate II
Posted on May 29, 2012 at 04:16

there is

http://www.gtk.org/features.php

aymen
Associate II
Posted on May 29, 2012 at 11:58

hi

i need the ''Resource Editor for Embedded GUI Library'', if you have a link please send me. thanks.

tecnico23
Associate II
Posted on June 05, 2012 at 10:38

Hi BJ Freeman,

Thank you for the link.

Do you use it to built an application that runs in a microcontroller? I can't understand how to make this. Where are the low-level files for microcontrollers?

Thank you very much,

Regards,

A.Paiva

tecnico23
Associate II
Posted on June 05, 2012 at 11:23

Hi Aymen,

Here you are. Make a searce by the name GUI and you will find it quickly.

http://www.st.com/stonline/stappl/resourceSelector/app?page=resourceSelectorPage&doctype=st_software_rsrc&ClassID=1734

Best regards,

A.Paiva