cancel
Showing results for 
Search instead for 
Did you mean: 

Coocox and the stm32f427vit6

jean_prieur
Associate III
Posted on September 12, 2013 at 11:33

Hello,

I was using Coocox and the STM32F407VGT6 and now I move to the new STM32F427VIT6. This microcontroller is not supported by Coocox, I have to select I'm using a STM32F407 but it works with that config (I can built, download code to flash, debug, ... everything is OK).

Do you know if it's unsafe to work with this configuration ?

Thanks !
2 REPLIES 2
Posted on September 12, 2013 at 15:47

There is no CooCox support presence here, you'll need to use their forum

You'd want to be using the most current version of the FW library, with support for 2MB

The limit with CooCox is likely to be an inability to write firmware into the second 1MB flash bank

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jean_prieur
Associate III
Posted on September 15, 2013 at 13:11

Hello Clive1, thanks for your reply, I will contact Coocox soon to ask for the STM32F427 support.

Have a good week !