cancel
Showing results for 
Search instead for 
Did you mean: 

Maximum output current of an OpAmp

jean_prieur
Associate III
Posted on May 04, 2012 at 17:05

Hello,

In datasheet, sometimes maximum output current is indicated (IsourceMin, Typ, Max), sometimes it is missing.

What is the best method to determine if an OpAmp can supply enough current to our load?

Thanks for the support,

Jean

#maximum-isink-isource #maximum-output-current #isource
1 REPLY 1
Nickname14663_O
Associate II
Posted on May 07, 2012 at 15:08

Dear Jean,

In most of datasheets, it is possible to find this information in the figures.

For example, here below there is the figure 6 of the TSV851 datasheet. 

It shows the output current vs the output voltage.

0690X00000602fyQAA.jpg

Thanks to this figure, you will be able to find the maximum current that the op-amp can sink or source.

Best regards,

Sylvain