2012-03-26 07:03 AM
Hi, I not having much success with using the UART (USART1) on my F4Discovery board (STM32F407). I am pretty new to STM32 and Keil (the IDE I am using). Here's my code:
&sharpinclude ''stm32f4_discovery.h''
&sharpinclude ''stm32f4xx_usart.h'' &sharpinclude ''stm32f4xx.h'' void usartSetup(void); void USART_PutChar(uint8_t ch);int main (void) {
usartSetup();USART_PutChar(0); //I realise this won't send a 0
USART_PutChar(8); //I realise this won't send an 8 USART_PutChar(255); //I realise this won't send a 255while (1) {
//loop forever } }void usartSetup (void) {
USART_InitTypeDef USART_InitStructure; //USART_StructInit(&USART_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); }void USART_PutChar(uint8_t ch) {
USART_SendData(USART1, (uint16_t) 0x49); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, (uint16_t) 0x49); }I'd be very grateful if someone could help. It never sends the 0x49 out of the UART1 TX (have checked pin PA9 and PB6) and then gets endlessly stuck on the while(USART_GetFlagStatus...). I am observing using the Keil debugger and see it get stuck in the while. I also have a scope probe on the TX pin and never see anything.
I am including the stm32f4xx_usart.c driver into the project.
Thanks!
#rs232-uart-usart-f4discover-407 #uart #stm32f4discovery2012-03-26 07:20 AM
Problems there with failing to enable clocks, or configure GPIO pins.
// STM32 USART1 (Tx PA.9, Rx PA.10) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1); // USART1_TX
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); // USART1_RX
}
/**************************************************************************************/
void USART1_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART1_Configuration();
while(1)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART1, 0x49); // Send 'I'
}
while(1); // Don't want to exit
}
2012-03-26 07:43 AM
Thanks for this, I didn't think you'd have to configure the GPIO if you were using just the UART (i.e. truning on the UART functionality I presumed would turn off the GPIO on the same pins).
I see a very gruesome trace out of PA9: I get the same track with either the MAX3232 chip connected or not. The PC interprets it a E9 (233).2012-03-26 07:58 AM
Dunno, is USART1 viable on the STM32F4 Discovery on these pins? Check the schematic.
Always assume the hardware isn't going to magically configure itself. Review some of the peripheral examples to get a feeling for how it's done, the API documentation mostly describes the functions, the reference manuals are the best place to understand the hardware. I've been using USART3, I had to mod this example to get you USART1. Here's a build using PB6,7 as the USART1 pins// STM32 USART1 (Tx PB.6, Rx PB.7) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* GPIOB clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1); // USART1_TX
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1); // USART1_RX
}
/**************************************************************************************/
void USART1_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART1_Configuration();
while(1)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART1, 0x49); // Send 'I'
}
while(1); // Don't want to exit
}
2012-03-26 08:22 AM
It works with the alternate pins (PB6 as TX). PA9 is connected to an LED which is why it is capacitively slowed and creates a nasty trace (might work at 1200baud :-).
Thank you for your help!2012-03-27 12:29 AM
Hello,
you can see on STMF4 Discovery user manual (page 34): on the PA9 there is a 4.7uF capacitor. If you want to use UART1 TX then you must remove this component and you must care about PC0, you must keep it HIGH. I suggest use UART6, the pins for UART6 is near to UART1 on the header. (PC6 Tx, PC7 Rx). cd3342012-03-27 03:59 AM
Hi
I am now trying to use PortE GPIO output, but it isn't doing as expected.// STM32 USART1 (Tx PB.6, Rx PB.7) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
void Delay(int ms);
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* GPIOB clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1); // USART1_TX
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1); // USART1_RX
// Configure Port E : Pins 7-15 as outputs
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOE, &GPIO_InitStructure);
}
/**************************************************************************************/
void USART1_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
/**************************************************************************************/
int main(void)
{
int i;
char c;
RCC_Configuration();
GPIO_Configuration();
USART1_Configuration();
i = 30;
while(i--) {
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART1, 0x49); // Send 'I'
//Load the byte onto pins 8-15 of Port E
//reset all 8 pins
GPIO_ResetBits(GPIOE, GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15);
c = i;
if(c & 0x01) {
GPIO_SetBits(GPIOE, GPIO_Pin_8);
}
if(c & 0x02) {
GPIO_SetBits(GPIOE, GPIO_Pin_9);
}
if(c & 0x04) {
GPIO_SetBits(GPIOE, GPIO_Pin_10);
}
if(c & 0x08) {
GPIO_SetBits(GPIOE, GPIO_Pin_11);
}
if(c & 0x10) {
GPIO_SetBits(GPIOE, GPIO_Pin_12);
}
if(c & 0x20) {
GPIO_SetBits(GPIOE, GPIO_Pin_13);
}
if(c & 0x40) {
GPIO_SetBits(GPIOE, GPIO_Pin_14);
}
if(c & 0x80) {
GPIO_SetBits(GPIOE, GPIO_Pin_15);
}
GPIO_SetBits(GPIOE, GPIO_Pin_7);
Delay(500);
GPIO_ResetBits(GPIOE, GPIO_Pin_7);
Delay(500);
}
while(1); // Don't want to exit
}
void Delay(int ms) {
ms = ms * 168000 / 4;
while (ms) {
ms--;
}
}
I see the I characters coming out of the RS232 but never see anything on PortE pin7 (or pins 8-15 for that matter). PortE_7 seems to be behaving like an input as well because if I connect it to a different board with a pin configured as an input but with pull-up, PortE_7 follows it to high.
2012-03-27 04:02 AM
Note: it is a while(1) as the last line of code not just while().
2012-03-27 07:00 AM
2012-03-27 07:50 AM
Sorry, should have spotted that.
Thanks for your help.