2013-09-12 02:49 PM
Hello,
I have problems to set up the right pin state while TIM2 is configured in PWM mode and turned off. The corresponding CC output pin stays HIGH while timer is off but I strongly need it to be LOW. I thought TIM_OCIdleState would solve this problem but it doesn't. Heres the initialization code: RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_2; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_TIM2); TIM_TimeBaseInitTypeDef TIM_TimeBaseStruct; TIM_TimeBaseStruct.TIM_Prescaler = 0; TIM_TimeBaseStruct.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStruct.TIM_Period = 103; TIM_TimeBaseStruct.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStruct); TIM_OCInitTypeDef TIM_OCInitStruct; TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStruct.TIM_Pulse = 80; TIM_OCInitStruct.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStruct.TIM_OCIdleState = TIM_OCIdleState_Reset; TIM_OCInitStruct.TIM_OutputNState = TIM_OutputState_Disable; TIM_OC3Init(TIM2, &TIM_OCInitStruct); /* --- Interrupt TIM1 CC Event --- */ NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 5; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 5; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_SetCompare3(TIM2,80); TIM_ITConfig(TIM2, TIM_IT_CC3, ENABLE); TIM_Cmd(TIM2, DISABLE); Is there a way to get the output pin low while the timer is not running? (btw., PWM works fine)2013-09-12 03:32 PM
Set the pulse width to zero (TIM2->CCR3 = 0) first?
2013-09-12 11:46 PM
Well, this works somehow, but it's not really a solution to my problem beacause as soon as I write to the CC register the output goes in high state, but I need the very fist PWM cycle to be exact! It has now a greater dutycycle than the others.
I think I could somehow workaround this problem but I just dont understand why this pin is high2013-09-13 04:35 AM
I just dont understand why this pin is high
Me neither, you should be able to control period/duty/phase without disabling the timer.2013-09-15 03:06 PM
Okay, got it, adding
TIM_OCxPreloadConfig(TIMx, TIM_OCPreload_Enable); does the trick 😉