2012-04-25 08:11 AM
This is my code for Transmission :
void USART3_tx(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable GPIOB and USART3 clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_USART3); GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_USART3); /* Configure USART Tx and Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_Init(GPIOB, &GPIO_InitStructure); /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control not enabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE); }int main(void){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); USART3_tx(); USART_SendData(USART3, 0xFF); while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) == RESET); GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_SET);}This is the code for Reception :void USART3_rx(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_USART3); GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_USART3); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_Init(GPIOB, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE);}int main(void){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_SET); USART3_rx(); while(USART_GetFlagStatus(USART3, USART_FLAG_RXNE) != RESET); while(USART_ReceiveData(USART3)!= 0xFF); GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_SET); GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_RESET);}I am using two Xbee modules with two STM32L-Discovery boards to realize this Tx - Rx.Kindly Help! #stm32l---discovery #usart #uart2012-04-25 11:22 AM
The RX code looks busted.
main()
{
// ... Init code
GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_SET);
USART3_rx();
do
{
while(USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == RESET);
}
while(USART_ReceiveData(USART3) != 0xFF);
GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_SET);
GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_RESET);
while(1); // do not exit
}
2013-04-29 11:59 PM
2013-04-30 04:39 AM
2013-05-08 03:51 AM
2013-05-08 04:29 AM
I would imagine generic C code for the protocol exists.
Couple of recommendations for code, use bytes for the data array, and front test TXE rather than back test TC.void SendArray(uint8_t *zeichen)
{
for(i=0;i<5;i++)
{
while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
USART_SendData(USART1, zeichen[i]);
}
}