2012-11-05 02:29 AM
Hello,
I designed a board which contains stm32f105 microcontroller, and i want to use DFU as bootloader in order to download my program to the micro controller through usb port. I put BOOT0 =1, and BOOT1=0 PA10=PD6=PB5=0 then i powered the circuit and connected it to usb port of my pc which runs windows xp. But the pc didn't recognise a new device. These are the processor data: STM32F105 VCT6 Z 990TD 93 MYS 99 045 First question: Why the pc didn't recognize a new device? Second question: the date code is 045 what year does this mean? Regards, Hisham2012-11-07 02:22 AM
Hello,
Finally the problem is solved. I connected pin 1 of the usb (power =5v) from computer directly to USB_VBUS pin PA9 in stm32f105 instead of connecting it through 20kOhm resistor and it works!