2012-05-21 06:16 AM
Hi everyone!
I'm new to the STM32 world, so I'm looking for some concrete example that USB OTG application with a STM32 uC.Did someone have sucess with a similar project that can be shared here?If however you can advise me to guide me, I would be thankful.2012-05-22 09:23 PM
Start from the USB library example. UM1021.
2012-06-22 03:14 PM
According to what i have read, just MSD and HID device drivers are developed. Does it mean that I still do can connect just MSD/HID devices to the STM32 USB Host?
There is someway to adapt the HID driver to a vendor-specific device? Is it so hard? I have no ideia.2012-06-22 04:36 PM
Doesn't it all predicate on your ability and knowledge about how to even interact with this custom device.
If you have no experience with programming USB devices, their device drivers, and the like, then yes you're going to have a bit of a learning curve ahead of you. Start by reviewing the sources supplied in the firmware libraries and see if it makes any sense within your current understanding of USB devices, and functionality.2012-06-23 07:05 AM
Thank you very much clive1;
But as a shortcut, if anyone has already managed to connect a usb device vendor-specific to the STM32, and could share here would be easier for me to find my path.Someone may have achieved.2012-06-23 09:25 AM
2012-06-23 10:14 AM
In this post to Keil forum, I wrote on the outline of class implementation for USB host using STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0
http://www.keil.com/forum/20569/ I examined v2.1.0 source, and I found just slight difference from above summary. If you open the spec of your target device, we can discuss on the implementation details, here. 1) How many interfaces does the device have - single or composite device? 2) How many endpoints and what is the transfer type/direction of each endpoint? 3) Does it use vendor requests? Tsuneo2012-06-23 11:28 AM
Actually, what Iwant to read as a USB device is other microcontroller Arm, a AT91SAM7S256. This ucontroller contains a USB 2.0 Full Speed machine. I need to use the USB because it is the unique physical access I have to it. It is embedded in a Lego NXT controller;
A similar work I have found is this:http://john.toebes.com/projects/first/46-samantha.html
; This module uses PIC32 (USB OTG) to connect to the NXT. Based on this work, could I adapt the used driver to the STM32?Through the USB Tracer I have read the information table below;Tsuneno, I am reading your post on Keil forum;Thanks clive1/chinzei.tsuneo!!
Parameter
Value
Hardware ID
USB\VID_0694&PID_0002&REV_0000
Setup Class
visaUsbDevice
Class GUID
{a3330edf-239d-4206-833b-1d58952613d5}
PDO Name
\Device\USBPDO-9
Service Name
WinUsb
</colgroup>
Parameter
Value
Connection Information
ConnectionIndex
0x4
CurrentConfigurationValue
0x1
Speed
0x1 (UsbFullSpeed)
DeviceIsHub
FALSE
DeviceAddress
0x3
NumberOfOpenPipes
0x2
ConnectionStatus
DeviceConnected
Pipe #0
Endpoint Descriptor
bLength
0x7
bEndpointAddress
0x1 [OUT]
bmAttributes
0x2 (USB_ENDPOINT_TYPE_BULK)
wMaxPacketSize
0x40
bInterval
0x0
Pipe #1
Endpoint Descriptor
bLength
0x7
bEndpointAddress
0x82 [IN]
bmAttributes
0x2 (USB_ENDPOINT_TYPE_BULK)
wMaxPacketSize
0x40
bInterval
0x0
Device Descriptor
bLength
0x12
bcdUSB
0x0200 (USB 2.0)
bDeviceClass
0x0
bDeviceSubClass
0x0
bDeviceProtocol
0x0
bMaxPacketSize0
0x8
idVendor
0x694 (Lego Group)
idProduct
0x2 (Mindstorms NXT)
bcdDevice
0x0
iManufacturer
0x0
iProduct
0x0
iSerialNumber
0x1 (0x409: 0016530703E2)
bNumConfigurations
0x1
</colgroup>
Parameter
Value
Configuration Descriptor
bLength
0x9
bDescriptorType
USB_CONFIGURATION_DESCRIPTOR_TYPE
wTotalLength
0x20
bNumInterfaces
0x1
iConfiguration
0x0
bmAttributes
0xC0 ( Bus_Powered Self_Powered )
MaxPower
0x0
Interface Descriptor
bLength
0x9
bInterfaceNumber
0x0
bAlternateSetting
0x0
bNumEndpoints
0x2
bInterfaceClass
0xFF (Vendor Specific)
bInterfaceSubClass
0xFF
bInterfaceProtocol
0xFF
iInterface
0x0
Endpoint Descriptor
bLength
0x7
bEndpointAddress
0x1 [OUT]
bmAttributes
0x2 (USB_ENDPOINT_TYPE_BULK)
wMaxPacketSize
0x40
bInterval
0x0
Endpoint Descriptor
bLength
0x7
bEndpointAddress
0x82 [IN]
bmAttributes
0x2 (USB_ENDPOINT_TYPE_BULK)
wMaxPacketSize
0x40
bInterval
0x0
2012-06-23 11:33 AM
2012-06-26 10:11 PM
Sorry for long delay,
For these days, I'm trying to download ''Bluetooth Development kit'' (BDK_Download1.zip) from Mindstorms support: Files site, http://mindstorms.lego.com/en-us/support/files/default.aspx but the download always stop at the first short portion. This kit should include a document of Bluetooth and USB protocols of NXT. A couple of data sheet sites have a copy of this document. ''LEGO MINDSTORMS NXT Communication Protocol'' I give up to download the original, though it's better to work on the original, for the latest version.. The USB protocol seems that a command (query) packet is sent over bulk OUT, and a status (reply) packet returns from bulk IN. No vendor request is used. Can you confirm it using a PC and a NXT, over a USB sniffer? Tsuneo