cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX v4.15.0 BUG Clocks not enabled

dennis23
Associate II
Posted on May 30, 2016 at 21:28

Hello again,

yesterday I updated to the newest version of CubeMX (v4.15.0) and since then in my project the clocks for the SDMMC and the STM32F746ZGT are disabled. In the pinout I selected the 4-Bit wide mode but the clocks are still off.

I tested it with a new project -> same result. In my VM I have an old v4.9.0 and in this version the clocks still working as expected.

Please can someone help? Is it a real bug?

 

 

EDIT: STM32F779 is still working on both SDMMC interfaces. The clock are enabled after I choose one of the configuration in the pinout tab.

#bug #cubemx #stm32f7
2 REPLIES 2
Walid FTITI_O
Senior II
Posted on May 31, 2016 at 11:39

Hi debegr,

It is already reported to our CubeMx team as an issue in the new version. Thanks for the feedback.

-Hannibal-

stm32cube-t
Senior III
Posted on June 14, 2016 at 08:46

Dear user,

Thank you for reporting this issue. It shall be fixed within STM32CubeMX 4.16 release.

Best regards.