2012-05-28 08:32 PM
Hi,
I have a couple of these:I am trying to get the on board ST-Link programmer to work with windows XP.I have installed the WinXP SW driver from here:And I'm having no luck, my board works fine on a Windows 7 machine, and the ST-Link utilty reports my device firmware as ''V1.J12.S0 JTAG Debugger''When I connect the device for the first time (or after deleting it's registry enum), Device Manager shows ST-LINK momentarily as an unknown device, then it vanishes, and only the USB Disk Drive ''STM32'' remains. The USB drive with the 3 web links on it works fine.I have tried the ST Visual programmer, the ST-Link utility, and CoFlash (Cocox), all say they cannot connect to the programmer.Any help would be greatly appreciated.Regards, Mick. #st-link-driver-xp2012-05-29 06:40 AM
2012-05-30 09:19 PM