2012-09-01 03:16 PM
Hello,
I am trying to write a byte(A0) to a particular location on the EEPROM. I have intialized the I2C(1) as in the code mentioned below(In sEE_INIT()). I write the byte using the EEPROM_write function and read the data from EEPROM_read function. However the program gets hung in the following while loop : while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)) in the EEPROM_read function. Could someone please let me know if there is some mistake i am making?Thanks in advance!#include ''main.h''#include ''constant.h''void sEE_LowLevel_Init(void);/** * @brief Initializes peripherals used by the I2C EEPROM driver. * @param None * @retval None */void sEE_Init(void){ I2C_InitTypeDef I2C_InitStructure; sEE_LowLevel_Init(); /*!< I2C configuration */ /* sEE_I2C configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = I2C_SLAVE_ADDRESS7; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = I2C_SPEED; /* sEE_I2C Peripheral Enable */ I2C_Cmd(sEE_I2C, ENABLE); /* Apply sEE_I2C configuration after enabling it */ I2C_Init(sEE_I2C, &I2C_InitStructure); }/** * @brief Initializes peripherals used by the I2C EEPROM driver. * @param None * @retval None */void sEE_LowLevel_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /*!< sEE_I2C Periph clock enable */ RCC_APB1PeriphClockCmd(sEE_I2C_CLK, ENABLE); /*!< sEE_I2C_SCL_GPIO_CLK and sEE_I2C_SDA_GPIO_CLK Periph clock enable */ RCC_AHB1PeriphClockCmd(sEE_I2C_SCL_GPIO_CLK | sEE_I2C_SDA_GPIO_CLK, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Reset sEE_I2C peripheral */ RCC_APB1PeriphResetCmd(sEE_I2C_CLK, ENABLE); /* Release reset signal of sEE_I2C IP */ RCC_APB1PeriphResetCmd(sEE_I2C_CLK, DISABLE); /*!< GPIO configuration */ /*!< Configure sEE_I2C pins: SCL */ GPIO_InitStructure.GPIO_Pin = sEE_I2C_SCL_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(sEE_I2C_SCL_GPIO_PORT, &GPIO_InitStructure); /*!< Configure sEE_I2C pins: SDA */ GPIO_InitStructure.GPIO_Pin = sEE_I2C_SDA_PIN; GPIO_Init(sEE_I2C_SDA_GPIO_PORT, &GPIO_InitStructure); /* Connect PXx to I2C_SCL*/ GPIO_PinAFConfig(sEE_I2C_SCL_GPIO_PORT, sEE_I2C_SCL_SOURCE, sEE_I2C_SCL_AF); /* Connect PXx to I2C_SDA*/ GPIO_PinAFConfig(sEE_I2C_SDA_GPIO_PORT, sEE_I2C_SDA_SOURCE, sEE_I2C_SDA_AF); }/* EEPROM write function*/void EEPROM_write(void){ I2C_AcknowledgeConfig(I2C1, ENABLE); I2C_GenerateSTART(I2C1, ENABLE); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1,0xA0, I2C_Direction_Transmitter); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(I2C1,0x00); // Send Year register address I2C_SendData(I2C1,0x6E); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_SendData(I2C1,0xA0); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_GenerateSTOP(I2C1, ENABLE); }uint8_t EEPROM_read(void){ uint8_t recieved_byte; I2C_AcknowledgeConfig(I2C1, ENABLE); I2C_GenerateSTART(I2C1, ENABLE); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1,0xA0, I2C_Direction_Transmitter); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(I2C1,0x00); // Send Year register address I2C_SendData(I2C1,0x6E); I2C_Send7bitAddress(I2C1,0xA0, I2C_Direction_Receiver); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); I2C_NACKPositionConfig(I2C1, I2C_NACKPosition_Current); I2C_AcknowledgeConfig(I2C1, DISABLE); recieved_byte = I2C_ReceiveData(I2C1);/* Send STOP Condition */I2C_GenerateSTOP(I2C1, ENABLE);while(I2C_GetFlagStatus(I2C1, I2C_FLAG_STOPF)); // stop bit flag}2012-12-03 09:42 AM
description
is
as
follows
2012-12-03 09:48 AM
I think as
description
is
as
follows
RCC_AHB1PeriphClockCmd(sEE_I2C_SCL_GPIO_CLK |
Maybe
AHB
2
PeriphClockCmd
well be correctsEE_I2C_SDA_GPIO_CLK, ENABLE);
There are two AHB buses?
2012-12-03 01:59 PM
APB1 & APB2
APB2
feed them
(etc
ADC3,
the USART1
TIM8
,
SPI1,
TIM1
, ADC2
ADC1
,
IOPG
,
IOPF
,
IOPE
,
IOPD
,
the IOPC
,
IOPB
,
IOPA
,
AFIO
)
Correct''
RCC_APB1
PeriphClockCmd(sEE_I2C_SCL_GPIO_CLK | sEE_I2C_SDA_GPIO_CLK, ENABLE);''
will be good
cause
#define sEE_I2C_SCL_GPIO_CLK RCC_APB2Periph_GPIOB
#define sEE_I2C_SDA_GPIO_CLK RCC_APB2Periph_GPIOBI2C EEPROM (STM M24lr64) problems
Notice:
Multi-
function pin only active ''I2Cx'' clock and don't remap or alternate function pin.
In I2C2 function, the USART3 clock
can not
enable simultaneity.
in the case: RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4 |RCC_APB1Periph_TIM3 |RCC_APB1Periph_USART3 <---can't apply this when active I2C2 at the same time.
, ENABLE );2012-12-03 02:13 PM
Correct
''
RCC_APB2
PeriphClockCmd(sEE_I2C_SCL_GPIO_CLK | sEE_I2C_SDA_GPIO_CLK, ENABLE);''
will be good
2012-12-03 05:58 PM