cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5-UDESTK Serial Console ?

sja
Associate II
Posted on September 23, 2014 at 15:46

I am using UDE 4.2.05 with the SPC560B-DIS (which has UDE debug hardware built in)

I can load and run code via JTAG but ...

How do I access the serial port connection to the target device ???

The target microcontroller UART is connected to the FTDI USB/serial/JTAG device but

I do not see a COM port show up on the PC for the target USB/serial connection.

Should this show up as a COM port or perhaps in a UDE window ??

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on September 24, 2014 at 10:59

Hello Adams ,

you can find in attachment a document how to install the driver :

Best regards

Erwan

________________

Attachments :

FTDI_Installation_driver_on_SPC560X_Discovery_board_cx369645_1.0_D2.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sb&d=%2Fa%2F0X0000000bZB%2FGShbxE0szlE8Amb7z3DQ1Ritv2kaXV0g8YUUrwBAm1E&asPdf=false

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee
Posted on September 23, 2014 at 17:01

Hello Adams ,

Take the driver inside PLS Tools

c:\Program Files (x86)\pls\UDE 4.2\Driver\JtagUsbDriver\

and

enable VCP in Device Manager(cf screenshot) for each driver

after rebooting the device .. you should see the COM PORT in your device manager

By default , the console UART is set to 38400 bauds.

Best regards

Erwan

________________

Attachments :

2014-09-23_165614.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sq&d=%2Fa%2F0X0000000bZC%2FZARwjO0UqHHwcSOhAh4V.z3Jistg2BuTZlp9Up8A1P4&asPdf=false
Erwan YVIN
ST Employee
Posted on September 24, 2014 at 10:59

Hello Adams ,

you can find in attachment a document how to install the driver :

Best regards

Erwan

________________

Attachments :

FTDI_Installation_driver_on_SPC560X_Discovery_board_cx369645_1.0_D2.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sb&d=%2Fa%2F0X0000000bZB%2FGShbxE0szlE8Amb7z3DQ1Ritv2kaXV0g8YUUrwBAm1E&asPdf=false