cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f4 internal pull down, external pull up

thommagn
Associate II
Posted on June 25, 2014 at 11:55

Hi,

I'm using an STM32F4 and have configured IOs as pwm outputs with internal pull down. These pins have been connected to an input of another chip which has a 5V pull up on its inputs. 

After some time the processor broke down. May this be the issue? I'm not quite sure I understand why, but I highly suspect this since its the only thing that was connected.
1 REPLY 1
John F.
Senior
Posted on June 26, 2014 at 09:19

Probably 5V got somewhere it shouldn't. Did the  microcontroller get hot? The pull-up pull-down currents are normally well below the ''latch-up'' currents which cause chip failure. Your circuit probably does not handle the interface properly. Get a hardware designer to look at it or post it here.