cancel
Showing results for 
Search instead for 
Did you mean: 

I2c on STM32f0Discovery

pietro2
Associate II
Posted on February 04, 2013 at 11:18

Good morning, i need to develop an application that read and write informations (like a mac address)between an stm32f0discovery board and a 24c02 EEprom, i need to use the PB8 and PB9 pins ad SCA and SCL.

If someone have suggestion like example codes or hardware setup are welcome.

Thanks.

#i2c-stm32f0discovery
1 REPLY 1
pietro2
Associate II
Posted on February 05, 2013 at 16:54

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6W1&d=%2Fa%2F0X0000000bpg%2F2WXZLVaHayXL6bV9xPMm0tGi3mmbtxYvDqdjJtIACj4&asPdf=false