2012-07-19 08:20 AM
Hi, I'm trying to play audio from flash, using your stm32f4_discovery_audio_codec andaudio_sample.c from project examples that comes with this board.
Here is my codeint main(void)
{
HardwareInit();
/*
xTaskCreate( vTaskLED1, ( signed char * ) ''LED1'', configMINIMAL_STACK_SIZE, NULL, 2,
( xTaskHandle * ) NULL);
*/
xTaskCreate( vTaskLED2, ( signed char * ) ''LED2'', configMINIMAL_STACK_SIZE, NULL, 2,
( xTaskHandle * ) NULL);
// GPIO_SetBits(GPIOD, GPIO_Pin_12 | GPIO_Pin_13);
EVAL_AUDIO_Play((uint16_t*)((uint16_t*) (&AUDIO_SAMPLE+58)), 990000-58);
vTaskStartScheduler();
for (;;);
}
I've taken audio sample from expample and changed it's to header file, otherwise it CoIDE couldn't compile it.
EVAL_AUDIO_SetAudioInterface(AUDIO_INTERFACE_I2S);
if (EVAL_AUDIO_Init(OUTPUT_DEVICE_AUTO, 50, 8000) == 0) {
GPIO_SetBits(GPIOD, GPIO_Pin_12);
}
This what I am doing in HardwareInit(); function.
Green led is lightning (which means that codec initialization became without errors), but I don't hear anything in my headphones.
Example project is working though.
Please, help me.
#me-too
2012-07-20 08:31 AM
Anyone? Is something that I've posted unclear or just no one knows?
2012-07-20 09:19 AM
Anyone? Is something that I've posted unclear or just no one knows?
No it's just uninformative. You've tried to port some example code into some other construct that looks like FreeRTOS, you've missed some critical steps, not really provided a complete context or code, and posted a code fragment which doesn't illustrate why it might have failed. You're basically asking people to guess what steps you missed in this process. Missing one is probably sufficient to break the whole. Perhaps there are other code dependencies, like interrupts, clocks, timers, SysTick, DMA, etc which are handled differently or not at all by FreeRTOS.
2012-07-23 05:07 AM
I've commented #include freertos.h ans tasks.h. It's just simple infinite loop in main function. And it is still doesn't work.
int main(void){ HardwareInit();/* xTaskCreate( vTaskLED1, ( signed char * ) ''LED1'', configMINIMAL_STACK_SIZE, NULL, 2, ( xTaskHandle * ) NULL); *//* xTaskCreate( vTaskLED2, ( signed char * ) ''LED2'', configMINIMAL_STACK_SIZE, NULL, 2, ( xTaskHandle * ) NULL);// GPIO_SetBits(GPIOD, GPIO_Pin_12 | GPIO_Pin_13);*/ EVAL_AUDIO_Play((uint16_t*)((uint16_t*) (&AUDIO_SAMPLE+58)), 990000-58);// vTaskStartScheduler(); for (;;);}So it's just initialization of codec which returning '0' to me (which I can see by green led lightning) and then EVAL_AUDIO_Play((uint16_t*)((uint16_t*) (&AUDIO_SAMPLE+58)), 990000-58); which doesn't work for some reasons.and infinite loop after it.2012-07-24 10:39 AM
So... What is unclear now? =(
2012-12-07 05:09 AM
Hi Michael,
Did you ever get this FreeRTOS integration to work? I am wrestling the exact same phenomenon since a couple of hours myself.. =) Edit: system_stm32f4xx.c turned out to be the culprit.2014-05-13 03:09 AM
Anyone could give me pointers on what was wrong with your code ?
I'm struggling with the same problem, everything seems fine, but no sound output at all ..thanks!2014-05-13 04:48 AM
2014-05-13 01:01 PM
This is the codec & PLL config i'm using
for a 48Khz playback, which looks exactlylike the config used in the example :/*------------------------------------CONFIGURATION: Audio Codec Driver Configuration parameters----------------------------------------*//* Audio Transfer mode (I2S Interrupt) *///#define I2S_INTERRUPT/* Audio Transfer mode (DMA, Interrupt or Polling) *///#define AUDIO_MAL_MODE_NORMAL#define AUDIO_MAL_MODE_CIRCULAR/* For the DMA modes select the interrupt that will be used */#define AUDIO_MAL_DMA_IT_TC_EN//#define AUDIO_MAL_DMA_IT_HT_EN//#define AUDIO_MAL_DMA_IT_TE_EN/* Select the interrupt preemption priority and subpriority for the DMA interrupt */#define EVAL_AUDIO_IRQ_PREPRIO 0#define EVAL_AUDIO_IRQ_SUBRIO 0/* Uncomment the following line to use the default Codec_TIMEOUT_UserCallback() function implemented in stm32f4_discovery_audio_codec.c file. Codec_TIMEOUT_UserCallback() function is called whenever a timeout condition occurs during communication (waiting on an event that doesn't occur, bus errors, busy devices ...). *///#define USE_DEFAULT_TIMEOUT_CALLBACK/* Enable this define to use the I2S DMA for writing into DAC register *///#define DAC_USE_I2S_DMA/*----------------------------------------------------------------------------*//************************* PLL Parameters *************************************//* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */#define PLL_M 25#define PLL_N 336/* SYSCLK = PLL_VCO / PLL_P */#define PLL_P 2/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */#define PLL_Q 7#define PLLI2S_N 258#define PLLI2S_R 32014-05-13 01:13 PM