cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F415 USB HS mode and CAN2

tony239955_stm1_st
Associate II
Posted on August 13, 2012 at 23:06

Using the MicroXployer the pin B13 was not allocated for the USB HS interface.

I wanted to use the CAN 2 bus interface.

Being that I am using the USB HS in FS  peripheral mode embedded in a 

product i.e.directly connected , do I need the VBus connection on B13(losing the CAN 2)?

Cheers

Tony

#usb-hs-vbus-can2
1 REPLY 1
flyer31
Senior
Posted on August 14, 2012 at 07:29

Yup, there is a very stupid clash between CAN2 and ULPI interface (although CAN2 has 2 pinning options, but only CAN2_TX does NOT clash with ULPI in one case - the other 3 cases (2xCAN2_RX, 1xCAN2_TX) clash with the ULPI databus, which has no second option, even in the highest pin devices).

It would be really nice of ST to consider a 3rd possibility for CAN2, NOT clashing with ULPI - if possible already in the 100 pin device. I think for people using CAN, it can be VERY useful to have two CANs available, especially in the case of a USB-HS interface.