cancel
Showing results for 
Search instead for 
Did you mean: 

stm32vl dicovery, ENC28J60, DS18B20

alv2005
Associate
Posted on July 26, 2012 at 15:19

I want to

make my first

project with

stm32vl

dicovery

.

I have a

network

controller

ENC28J60

(http://www.ebay.com/itm/New-ENC28J60-Ethernet-LAN-Network-Module-Schematic-For-Arduino-51-AVR-LPC-STM32-/350499598396?pt=LH_DefaultDomain_0&hash=item519b67703c)

and temperature

sensors

 

DS18B20

.

I want to

make the

sending sensors data

to the web

server.

Where can I find

examples of

operating

such a project

?

Thanks

#http #stm32vl-dicovery-enc28j60-ds18b2 #tcp/ip #1-wire
4 REPLIES 4
Posted on July 26, 2012 at 18:45

Got any experience coding similar apps on a PC or anything?

You should start by looking to the vendor of such boards, and then the internet in general. If their are any canned packages that do what you want they'll likely show up on Google or Bing,

Perhaps something like LwIP.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist
Posted on July 27, 2012 at 00:51

''I want to

make the

sending sensors data

to the web

server''

 

There are two separate sub-systems here:

1. Interfacing to the sensors & taking readings;

2. Transferring data to a web server.

Maxim provide plenty of examples and application notes for using their 1-Wire (TM) sensors, and google will find plenty of others.

eg,

http://www.8052.com/forum/read/95905

Communicating with a web server will require you to implement  TCP/IP and a web Client; ie, an HTTP client.

This is an excellent HTTP tutorial:

http://www.jmarshall.com/easy/http/

ST provide TCP/IP examples - including InterNiche and other Open-Source stacks - and google will find many, many more...
alv2005
Associate
Posted on July 27, 2012 at 08:49

My experience- project with Arduino. It seems to be to work hard ...

Thanks for links

dannym
Associate II
Posted on August 03, 2012 at 23:28

Arduino is very close to C, if you were able to translate it, you'd just need to set the clock speeds, pins, and SPI peripheral for compatible use.

There IS a project to bring Arduino to the STM32 directly, I don't know what the state of usability is.  I suggest you google it.

The ENC28J60 is a stand-alone Ethernet controller in itself.  It will do the job, through the SPI port.  However, the STM32F4 Discovery has its OWN Ethernet hardware peripheral, however, you'd need a hardware phy to adapt the voltage and current.  The DP83848 

http://www.ebay.com/itm/260868624339?ssPageName=STRK:MEWNX:IT&_trksid=p3984.m1439.l2649#ht_1615wt_1169

 would do that.  I expect the STM32 peripheral library would have a ready example for running ethernet through that phy.

Ironically, it costs more than an ENC28J60 module, even though it is only a phy, not a phy plus controller.  However, working through the SPI on the ENC28J60 is probably far more limited than using the STM32 peripheral for bigger projects, and you won't learn as much about ethernet by using the ENC28J60.  But, like I say, the ENC28J60 is completely adequate for reading temperature sensors.