2012-12-15 11:00 AM
Hello everyone,
I am experiencing something strange with the use of USART1 on a STM32F103 in order to decode some stream coming from a RC Receiver. The behaviour I am getting is that once initialized, the first data will come to the IRQ of usart. the RXNE_FLAG will be set on the first char of the packet. I will get another IRQ for the second char, but the RXNE flag will no be set at this time. is this normal ? I thought i should get a flag set for every byte and that using USART_receive would clear the flag. am i wrong ? I guess that as long as I am only setting the RXNE interrupt, the IRQ handler will only be called when there is a char, but i was wondering if this behaviour was normal and if not what could be a reason for this. just to make sure I have put the code I am using here in case theer is something i do wrong. Thanks for your comments 🙂 Lionel.2012-12-15 11:48 AM
Well you should get an interrupt per byte, and clear it byte reading the data register.
You might get framing or parity errors also. The M3 can potentially re-enter an interrupt routine if the last thing it does is clear an interrupt. Pipelining, and bus delays can cause the source to remain asserted briefly, but enough to tail-chain back in. If you do some actual work, like writing the character to a fifo/ring buffer that will be sufficiently consuming. The re-entry condition will appear not to have any interrupts set in the USART/whatever, and you can just exit without doing anything. If the interrupt continually re-enters, something is still asserted, check the interrupt/status registers for the potential cause.