cancel
Showing results for 
Search instead for 
Did you mean: 

Two Shunt Resistors

jove
Associate
Posted on September 27, 2012 at 19:57

Hello. I'm trying to develop bldc motor driver with referecing MClib.

My question is why the current is sensed with three shunt resistor? 

The document,UM1052 descibed as the current sensing is sufficient sample only two currents.

Is it possible to use two shunt resistors, for Ia and Ib, with MClib?

1 REPLY 1
bille.stello
Associate II
Posted on November 12, 2012 at 16:24

It is, but you need to apply some modification to the code.

Due to switching noise, using only two resisitors results into a limitation of the maximum SVPWM modulation index (i.e. it's not possible to read with 100% duty cycle).This is often not acceptable.

Best Regards,

Billino