cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L151F3 Bootloader

beatle7
Associate
Posted on June 24, 2013 at 13:13

Hello!

Have anybody any information on bootloader interface configuration for I couldn't find direct instructions on port connections. I assume they should be PC2 and PC3 pins (due to SYSCFG->RMPCR1 default value) but there is some problem: STM8LF151F3 in UFQFPN20 package have no these pins.

So is it even possible to use bootloader in UART mode with this package or I should look towards usin SPI interface? By the way, which pins do bootloader require for SPI? Maybe PB5, PB6, PB7 ?

#bootloader
1 REPLY 1
florian2399
Associate
Posted on May 06, 2014 at 11:10

Hi,

did you find any answer to your question yet? We are stuck at the exact same point trying to use the STM8L151F3's bootloader.

Best Regards

Florian