cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F051 analog comparator?

asrock70
Associate II
Posted on November 09, 2012 at 15:59

What is the

input

resistance of the

analog

comparator

in STM32F051?

I can not

find

this information

in the Datasheet.

2 REPLIES 2
frankmeyer9
Associate II
Posted on November 10, 2012 at 18:13

I can not

find

this information

in the Datasheet.

Me neither, seems it is not specified.

I suggest to contact a local sales/support administrative.

For bravity, I would assume a value in the range of the ADC input resistance.

Posted on November 10, 2012 at 19:50

Table 50 indicates a leakage value of 0.2uA for input set to analog.

On the other hand, Fig. 23 indicates 1uA for the ADC input, which together with the specified max. 50kOhm source impedance yields a 50mV error. Now that's more than 50 LSB... I would love to hear ST's explanation for that.

JW