cancel
Showing results for 
Search instead for 
Did you mean: 

Comparator in STM32F373?

asrock70
Associate II
Posted on January 19, 2018 at 10:34

Hello i have any question about Comp in STM32F3

1. W

hat is the p

ropagation delay for low overdrive, for example 5mV? In DS is only for 100mV. For High speed mode.

2. W

hat is the output current for Low and high level on output commparatar?

3. What is the large-signal differential voltage amplification?

4. If is used internal DAC for driving one comparator input, can be used DAC without buffer?

0 REPLIES 0