cancel
Showing results for 
Search instead for 
Did you mean: 

Has STM32 MC FOC SDK V3.3 released?

tamil
Associate II
Posted on December 13, 2012 at 00:37

Hi,

I noticed that  STM32 MC FOC SDK V3.3 was mentioned in ST Motor Control Workbench V2.1 as one of the target libraries. I also found a

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/RELEASE_NOTE/DM00068242.pdf

mentioning it. But, I couldn't find it being available for download on ST.com. Has it indeed released? If so, where can I find it?

Thanks,

Tamil
3 REPLIES 3
Gigi
Senior
Posted on December 13, 2012 at 09:50

Ciao Tamil,

The v3.3 is up to now released in

confidential distribution

. So you have to ask it to local ST support office.

The WEB distribution will be released soon.

Ciao

Gigi

tamil
Associate II
Posted on December 13, 2012 at 22:38

Thanks for the info Gigi!

-Tamil

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards