cancel
Showing results for 
Search instead for 
Did you mean: 

Announcement: Makefiles for building every STM32 Library under Linux using GCC.

rick23
Associate II
Posted on September 24, 2015 at 23:16

Hi,

  This is to announce a set of Makefile's that aim to build every STM32 Library under Linux using GCC.  Comments are welcome.

  Please see

https://github.com/rickbronson/GCC-Makefile-for-Building-STM32-Libraries for more info.

  Cheers,

  Rick

#gcc-linux
2 REPLIES 2
onderdelen
Associate II
Posted on September 27, 2015 at 16:14

Hi,

your aim is a noble effort! However, gnu makefiles are a pain to maintain and extend beyod a small project (I speak from experience).

A better alternative is CMake. I've successfully used CMAke for building STM32 firmware on FreeBSD  for many years.

[small excerpt from CMake output for STM32L0] :

Scanning dependencies of target SunnaBat.elf

 

[ 93%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/opslag/home/ewout/techniek/projecten/swexternals/STM32/HALLibraries/Processor/stm32l0driver.cpp.o

 

[ 93%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/opslag/home/ewout/techniek/projecten/swexternals/microprocessor/syscalls.cpp.o

 

[ 94%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/beheer.cpp.o

 

[ 95%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/beuk.cpp.o

 

[ 95%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/init.cpp.o

 

[ 96%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/meet.cpp.o

 

[ 96%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/regel.cpp.o

 

[ 97%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/rtos.cpp.o

 

[ 97%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/stm32l0.cpp.o

 

[ 98%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/stm32l0ISR.cpp.o

 

[ 98%] Building CXX object toepassing/CMakeFiles/SunnaBat.elf.dir/sunnabat.cpp.o

 

[ 99%] Linking CXX executable SunnaBat.elf

 

[ 99%] Built target SunnaBat.elf

 

[100%] SunnaBat.elf is gemaakt. Hier volgt informatie over het ELF bestand.

 

SunnaBat.elf  :

 

section             size        addr

 

.text              49780   134217728

 

.eh_frame              4   134267508

 

.ARM.exidx          1176   134267512

 

.rodata             3824   134268688

 

.data                 40   536870912

 

.bss                5720   536870952

 

._usrstack           152   536876672

 

.comment             112           0

 

.debug_aranges      4232           0

 

.debug_info       626377           0

 

.debug_abbrev      37847           0

 

.debug_line        58707           0

 

.debug_frame       18160           0

 

.debug_str         71704           0

 

.debug_ranges       3840           0

 

.ARM.attributes       40           0

 

Total             881715

 

CMake is fantastic and very easy to configure.

If you need tips about it ask around!

Ewout Boks

rick23
Associate II
Posted on September 28, 2015 at 05:58

  In general I agree.  I've struggled with makefiles myself.  But in this instance the makefiles are very simple and tiny.  The issues here are more about fixing up the wrong case issues (I guess the library assumes it's being built in MSDOS), inconsistency in directory structure names across different chip families and tweaking of loader scripts.  Don't think cmake will help with those issues.  Appreciate your input.

  Rick