2017-04-18 02:07 PM
Hi Forum,
I'm using the stm32f091, but when I enable the USART3 interrupt, the system hard faults. I already use USARTS1 and 2 without any problem. Not sure what else is required, so I'd be grateful for some assistance. One thing I;d like to know is how do you distinguish between interrupts from USARTS3 up to USART8.
Kind Regards
Bob
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // Enable GPIOC clock RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); // Enable USART3 APB clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); // Connect pin to Periph GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_1); // USART3 TX GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_1); // USART3 RX // Configure pins as AF pushpull GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOC, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE); // Enable the COM3 Receive interrupt: this interrupt is generated when the// COM3 receive data register is not empty USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);// USART3 IRQ Channel configuration
NVIC_InitStructure.NVIC_IRQChannel = USART3_8_IRQn;NVIC_InitStructure.NVIC_IRQChannelPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);2017-04-18 03:23 PM
2017-04-18 04:17 PM
Fair enough regarding the usart article status register but any idea why the hard fault occurs.
Bob
2017-04-18 06:25 PM
Make sure the ISR's name matches that in the vector table, typically located with startup code.
JW
2017-04-18 07:17 PM
Are you sure it is getting a Hard Fault, and not just entering the Default Handler, which is also a while(1) loop?
Check the naming of your IRQHandler, and that it matches, and links properly with the entry in the Vector Table.
2017-04-19 05:38 AM
Thanks very much. The interrupt was missing from the vector table. Adding it fixed the issue. Once again many thanks to the forum.
Kind Regards
Bob