2013-01-02 02:09 PM
Hi all,
I have a strange behaviour with 4 stm32f407 boards related to the jtag. The jtag of the stm32f4 is connected to a FTDI4232 chip. I have connected only the JTCK (with a 10k pd), the JTDI (with a 10k pu), the JTDO (with a 10k pu) and the JTMS (with a 10k pu). The NJTRST pin is reconfigured at the reset as the SPI MISO function. To program the FLASH I use an openocd script. Everything worked fine for month and suddenly, I cannot reprogram the FLASH. In my new software release, I use the instruction wfi (when the kernel runs the idle process) and I have reconfigured the GPIO pin handling the NJTRST. Time to time the programming process is operational, but this happens 1 every 10000 tentative :(
The programming operation is done with boot0 connected at 3.3V and boot1 fixed on the pcb at gnd.
What can I try for recovering again the control of my systems? The silicon revision is A.
Thank you for your advise.
Best regards
Rom. #jtag #flash #stm32f407 #openocd2013-01-02 03:52 PM
Do you have a good power-on-reset circuit, and can you clamp NRST/NRESET low on you programming header to get an effective and repeatable reset?
2013-01-03 01:13 AM
Hi Clive1,
Thank you for your suggestions. You put me on the tracks and I was able to figure out the problem. The pin NJTRST was float!! With the scope I discovered that the level was close to gnd. I have just pulled up properly the pin and everything work fine!
Thank you again for your help,
Regards
Rom