2013-12-05 07:43 AM
Hi,
I have two timer running TIM2 and TIM4. I would like to capture TIM4 counter value when TIM2 overflows (update). I do not wish to sample the value inside the ISR because i need precision. I would like to use something like an input capture but with the trigger being the TIM2 update instead of an outside event.I feel like there is a simple solution there but just can't see it. Anyone has done that before?Thanks,Justin #stm32-timer-capture-update2013-12-05 09:01 AM
2013-12-05 10:37 AM
Yes it looks like i'll try that.
Setup DMA1 CH2 to get triggered by TIM2_UP then the DMA transfers the value from TIM4->CNT to a RAM location later read is the TIM2_UP ISR...Thanks