cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet Communication

aru
Associate II
Posted on February 20, 2013 at 06:33

I am using STM32F107RB for Ethernet Communication. If i am using only one STM32F107RB module there is no problem but when i connect two modules to two different systems via modscan32, one of the module responds properly and the other module does not responds, and after some time the other modules responds properly but the first module hangs up. This process continuous every time...

The corresponding code has been attached, please go through it and let me know where this problem can be tackled......

Thanks in advance........

#time-waster #cross-post #do-it-right
13 REPLIES 13
chethurocks
Associate II
Posted on February 20, 2013 at 08:03

Even i'm facing the same problem...

frankmeyer9
Associate II
Posted on February 20, 2013 at 09:32

Could the boards have the same (default) MAC address ?

Posted on February 20, 2013 at 13:30

MAC address, and fixed IP address? Both pretty basic Ethernet and TCP/IP concepts.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist
Posted on February 20, 2013 at 15:16

Same question on the Keil forum had already received the same answer yesterday:

http://www.keil.com/forum/22357/

Posted on February 20, 2013 at 16:20

Forget Zombies, the Unthinking Living scare me...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
aru
Associate II
Posted on February 21, 2013 at 05:28

Thanks for all of u..... i am given the same mac address that is problem......

aru
Associate II
Posted on February 21, 2013 at 05:29

Thanks for all of u..... i am given the same mac address that is problem......

Andrew Neil
Evangelist
Posted on February 21, 2013 at 14:12

How about also acknowledging the reply you received to your original post in the Keil forum?

chethurocks
Associate II
Posted on February 26, 2013 at 08:10

Hi, 

    Is there any way of assigning the IP address Dynamically(as it is done in the computers network configuration).... If it is possible then could you please tell me about that thing......

Thanks in advance ..........