cancel
Showing results for 
Search instead for 
Did you mean: 

Dual ADC frustrating Me (I need Urgent Help!!)

bluewaters213
Associate III
Posted on February 12, 2013 at 21:37

The original post was too long to process during our migration. Please click on the attachment to read the original post.
2 REPLIES 2
Posted on February 12, 2013 at 21:51

I'll take a pass.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
raptorhal2
Lead
Posted on February 13, 2013 at 03:38

Two channels per ADC and no DMA ? Perhaps you are not showing everything relevant.

A 10K input impedance with 1.5 cycles sampling will always be inaccurate.

Start with the Standard Peripheral Library and the Dual ADC example there so you have a working reference and so we can understand what you are doing.

Cheers, Hal