cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 Discovery JP1 (STLINK USART RX,TX)

javanzee
Associate
Posted on February 05, 2013 at 01:35

What is the purpose of JP1?  It connects to the STLINK MCU, and via two solder-jumpers on the bottom of the board (SB14,15) to PA9,10 of the 'F051 (the USART-1 pins).  Can the STLINK enumerate as a CDC endpoint, and thus provide a serial port for the 'F0?  Or, perhaps it is there to explore the built-in hardware bootloader (again enumerated as a CDC endpoint)? If either of these speculations is true, would the STLINK MCU first need to be re-programmed as a CDC device via the DFU loader?

0 REPLIES 0