2013-04-27 08:53 AM
2013-04-27 11:09 AM
The address increments by two because 16-bit contains TWO 8-bit bytes. The address inside the CPU is for bytes. It is a byte offset.
You know you can read/write to it like normal memory? uint16_t *p = (uint16_t *)0x64000000; // As a pointer to 16-bit WORDS p[0] = 0x1234; p[1] = 0x5678; p[2] = 0x9ABC; p[3] = 0xDEF0; printf(''%04X\n'',p[0]); printf(''%04X\n'',p[1]); printf(''%04X\n'',p[2]); printf(''%04X\n'',p[3]); uint8_t *q = (uint8_t *)0x64000000; // As a pointer to 8-bit BYTES printf(''%02X\n'',q[0]); printf(''%02X\n'',q[1]); printf(''%02X\n'',q[2]); printf(''%02X\n'',q[3]); The RAM should extent 0x64000000..0x647FFFFF ie through p[0x3FFFFF] or q[0x7FFFFF]2013-04-28 12:11 AM
Thank you Clive 🙂
I understand a little more now. I have do this test : void test_Clive_ram(void) { uint8_t ReadRam[4] = {0}; uint16_t *p = (uint16_t *)Bank1_SRAM2_ADDR; // As a pointer to 16-bit WORDS uint8_t *q = (uint8_t *)Bank1_SRAM2_ADDR; // As a pointer to 8-bit BYTES p[0] = 0x1234; p[2] = 0x5678; p[4] = 0x9ABC; p[6] = 0xDEF0; ReadRam[0] = q[0]; // Result is : 0x34 ReadRam[1] = q[1]; // Result is : 0x12 ReadRam[2] = q[2]; // Result is : 0x78 ReadRam[3] = q[3]; // Result is : 0x56 } I see that the data are LSB first ... My point was to use the PSRAM as a little buffer for a TFT screen (SSD1963 480 x 272). I get the rest of the components and will be able to use the board i have made at end of the week day's. As i understand a little more now i will have to use a step of 2 for the address because the data i have to send to the screen controller are in 16bits. It's just 2M x 16bits but better than nothing ..... I will have to look how the DMA work and prey that it can handle a step of 2 for the address too so i can use it in background to send pixels continuously to the screen 😉 You can see the old board i made here :http://www.youtube.com/watch?v=tx9YSFPpKLw&list=UUPP_IrS9eBG80PxEURo0Ctw&index=1
I made hw mistake with the memory and cant use it on that board. It use a Core407i from waveshare. The actual board i use is the HY-STM32F4xxCore144 from here :http://www.hotmcu.com/hystm32f4xxcore144-coredev-board-p-10.html
So i don't have to solder any memory and don't made error again 😉 Anyway many thanks for your advice and i hope that my Frenglish language is not too bad. Cheers.2014-02-25 04:54 AM
Hello darth,
did You use the HY_Board? I run into trouble use that board with stemwin gui and the ps ram. It is hard to debug because the trouble seems to be in the precompiled lib.