cancel
Showing results for 
Search instead for 
Did you mean: 

Adding RAM to STM32F4

khouja_houssem
Associate II
Posted on September 04, 2013 at 21:37

Hi,

For my project I need additional RAM, is it possible to add memory to the STM32F407VG (in the STM32F4-Discovery Board) using the FSMC interface?

3 REPLIES 3
Posted on September 04, 2013 at 21:58

Review schematics and pin allocations for boards using external memory, like STM3240G-EVAL or RedDragon407

Look also for daughter boards which you can plug the STM32F4-Discovery into.

Personally I'd be looking for a different board, with a higher pin count STM32 part to better accommodate the DCMI and FSMC interfaces. Check eBay, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
khouja_houssem
Associate II
Posted on September 04, 2013 at 22:19

Thanks for your answer CLIVE1.

In the STM32F4-Eval board we have only 8 address outputs (A16 to A23). 

What can be the maximum memory they could controle? Can it reach 16MB?
Posted on September 04, 2013 at 23:24

About 256 or 512 bytes depending on if your data bus is 8 or 16-bit wide?

I haven't looked at the STM32F4-Discovery being a practical platform for external memory, depending on the memory you'd have to wire up ~30 pins. The camera would be another ~20 pins

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..