cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.14.0/4.15.0 BUG: Target/IROM settings are NOT preserved

Posted on January 20, 2016 at 10:16

Hi,

Whenever I regenerate the code using STM32CubeMX the new (re-generated) Keil project has Target/IROM1 Memory Areas overwritten  e.g.

I usually use RAM area are for IROM1 for debug purposes

and the IROM1 is set to:

Start: 0x20000000, size:0x1000

After regenerating the code the

IROM1 settings are overwritten and  now I see:

Start: 0x8000000, size:0x10000

Is there any way to make STM32Cube preserve Keil Target/IROM settings?

Please note Target/IRAM settings are preserved. It looks like a bug.

Bogdan

1 ACCEPTED SOLUTION

Accepted Solutions
Nesrine M_O
Lead II
Posted on April 04, 2016 at 16:43

Hi golab.bogdan,

Thank you for your feedback. The issue has been reported internally.

-Syrine-

View solution in original post

7 REPLIES 7
Posted on April 03, 2016 at 10:12

The bug is still present in 4.14.0

Posted on April 03, 2016 at 10:13

Is there any way to make ST developers aware of this issue?

Nesrine M_O
Lead II
Posted on April 04, 2016 at 16:43

Hi golab.bogdan,

Thank you for your feedback. The issue has been reported internally.

-Syrine-

Posted on May 23, 2016 at 12:06

Hi Syrine,

Unfortunately the issue was NOT fixed in the CubeMX 4.15.0. The IROM setting are still altered after re-generating the project using CubeMX.

Thanks,

Bogdan

Posted on November 07, 2016 at 17:47

Hi,

I wonder if there any plans to fix the issue. I see the problem also in 4.17.0,

Bogdan

Posted on February 03, 2017 at 13:50

It seems that the issue is fixed at least in 4.19.

Thank you

Bogdan

Alex Ivanov
Associate
Posted on June 03, 2017 at 07:23

The same error for STM32F745!!! ver. 4.21.0