2013-02-27 03:03 AM
Hi
Is there a example project or somethin similar I can use as a foundation to use the stm32f4 discovery as a usb audio device? I want to stream the data of the on-board or an external mems microphone using the i2s (with dma) interface via usb to a host pc. I'm new to STM32 devices and all the specifics, although I already have good experiences with TI devices. #i2s #usb2013-02-27 06:51 AM
Have you waded through the fw examples for the DISCOVERY and EVAL boards? Not sure there something that does everything you want, but there are probably some usable parts in them.
2013-02-27 07:43 AM
Thanks for your reply. Of course I found the ''Audio_playback_and_record'' example project but I guess there is not explained how to configure the eval board as an usb audio device. I know how to configure the usb descriptors but I need to know how to configure the stm32 usb device stack to get the data from the I2S (with DMA) to the host.
2013-02-27 08:02 AM
2013-02-27 08:59 AM
This sounds interesting but the st side is somewhat confusing. Where can I get this piece of software?
2013-02-27 10:18 AM
Hi,
Probably is your best bet, together with the I2S driver provided by ST. Regards, Chris2013-02-27 10:38 AM
Thanks for your reply. This looks interesting but meanwhile I found the file clive1 had suggested. Unfortunately both of your suggestions are for usb audio speakers. But I need usb audio microphone and from my own experiences I know that it is a little bit complicated to rewrite a speaker example into a microphone one.
So I am
still
grateful for any help
. EDIT: I found this very interesting thing but unfortunately there is no firmware for download http://www.st.com/web/catalog/tools/FM116/SC1116/PF2535832013-02-28 02:06 AM
Hi,
I understand what you need, but the chance to find complete project with source code for this via Google are almost zero. Maybe something for Linux, but no way to find this with working Windows driver and source code for it. The ST example for the microphone is basically an I2S driver that stores the data to a USB flash disk, then it can play this data. There is no emulation of USB audio device that will show as USB microphone when plugged to a computer, or at least i haven't seen this one in the examples. The project link seems to fit what you need, but will require some work:SDR-Widget is an interface based on the Atmel AT32UC3A3 microcontroller that provides the following functionality to SDR circuits such as the SoftRock. A branch of the project called audio-widget provides a USB-I2S module and various Analog Boards (AB) for audiophile USB-DAC playback.
sdr-widget:
2013-02-28 07:29 AM
I think it's not that complicated to realize what I need but I would need a starting point. For using my stm32 board as an usb audio microphone, I need the following chain
MEMS mic -> I2S -> DMA -> USB stack -> USB peripheral -> host pc I've implemented exactly that with an TI stellaris lm3s9b92. But I needed to fit the TI usb stack and that was some work. Now I want to migrate my project to the stm32f4 because of the fpu und more performance. The USB microphone is actually only there to verify the correct functionality of the the whole chain.2013-03-22 11:07 AM
Have you been able to get good audio quality from the built-in MEMS mic? I find the audio quality very disappointing using the ST example program, not sure if this due to the program or the board. Do you have any idea where the problem lies?