2013-06-17 08:07 AM
hello people
i'm using IAR IDE and i'm trying to make a program which get accelo values (x and y) and put them on lcd this is my code and it didnt work i dont know why: ****************************** #include ''stm32f4xx.h'' #include ''LCD2x16.c'' char SPItransaction (int AandD) { // about 7us #define MOSI 0x8000 #define MISO 0x4000 #define SCK 0x2000 #define SEL 0x1000 int Ret = 0; GPIOB->ODR &= ~SEL; // SPI select for (char k = 0; k<16; k++) { // for 16 bits if (AandD & 0x8000) GPIOB->ODR |= MOSI; // send address & data else GPIOB->ODR &= ~MOSI; // AandD <<= 1; // next bit of address & data GPIOB->ODR &= ~SCK; // SCL lo for (int i = 0; i<100; i++) {}; // waste 150ns Ret <<= 1; // shift bits read right GPIOB->ODR |= SCK; // SCL hi if (GPIOB->IDR & MISO) Ret++; // read bit and add to string }; GPIOB->ODR |= SEL; // SPI done return ((char)(Ret & 0xff)); // return result } void SPIwrite(int Adr, int Data) { SPItransaction(((Adr & 0x3f) << 😎 + Data); // prepare 16 bits } char SPIread(int Adr) { char Ret = SPItransaction(((Adr & 0x3f) << 😎 + 0x8000); // 16 bits return (Ret); // return result } void main () { // ports init: 15-MOSI, 14-MISO, 13-SCK, 12-SEL RCC->AHB1ENR |= 0x00000002; // Enable clock for GPIOB GPIOB->MODER &= ~0x80000000; // PB 15 => input pin, no AF! GPIOB->MODER |= 0x45000000; // PB 15,13,12 => outputs GPIOB->ODR |= 0xc000; // SEL & SCK -> hi // Init accelerometer chip SPIwrite(0x20, 0xc7); // CR1: power-up, all axes SPIwrite(0x21, 0x40); // CR2: Block data update & 12 bit mode SPIwrite(0x22, 0x00); // CR3: no filtering // Init LCD & prepare display LCD_init(); // Init LCD LCD_string(''x= mg'', 0x00); // prepare 1st row LCD_string(''y= mg'', 0x40); // prepare 2nd row // endless loop while (1) { short retX = SPIread(0x29) + (SPIread(0x2a) << 8); // x axis, both bytes LCD_sInt16(retX, 0x02, 1); // display result short retY = SPIread(0x2b) + (SPIread(0x2c) << 8); // y axis, both bytes LCD_sInt16(retY, 0x42, 1); // display result //for (int i=0; i<100000; i++) {}; // waste time, ~30ms }; } the lcd works just the values always are 0! i think the problem is in the registeries , help plz2013-06-17 11:47 PM
You will have a hard time to find some one to support you with this
https://en.wikipedia.org/wiki/Magic_number_%28programming%29
and register-hack ridden code. I'm not going to dig into it. Why bit banging ? All STM32's have native SPI peripherals.2013-06-18 01:15 AM
okay forget about that code.
Can u help me and put a working code with IAR? and thnx 🙂2013-06-18 02:46 AM
okay forget about that code.
Good idea. Had you ever to maintain such a code ... ? But more important : which accelerometer ?