cancel
Showing results for 
Search instead for 
Did you mean: 

help STM32-P103 RS232

mustapha_menhou
Associate II
Posted on March 25, 2013 at 22:18

Hi i

 would like

to use the circuit

MAX3232

(

RS232

adapter

) to connect two 

PORT

RS232

with this

 circuit 

using just

TX and RX

only

if possible

this experience?

?

?

?

?

and thank you 
4 REPLIES 4
Andrew Neil
Evangelist
Posted on March 25, 2013 at 23:02

There seems to be a language barrier here. Perhaps it would be easier to explain your requirement with a diagram...?

mustapha_menhou
Associate II
Posted on March 26, 2013 at 00:15

Here is a

PDF

that

represents

my problem

if

possible to do this

configuration?

??

________________

Attachments :

Doc1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1An&d=%2Fa%2F0X0000000bjO%2FMxvFcOji_FYohzLHw5WB39F3L3WIkazQ.unp2P0.vmY&asPdf=false
Andrew Neil
Evangelist
Posted on March 26, 2013 at 07:47

By ''STM32-P103'' I assume you mean this:

https://www.olimex.com/Products/ARM/ST/STM32-P103/

Note that it has one RS232 port already - so you only need to add one other.

Study the documentation to see where the other UART port pins can be accessed on the various connectors on the board...

Andrew Neil
Evangelist
Posted on March 26, 2013 at 09:31

I see you have also posted the same question in a different thread:

/519d41ef