cancel
Showing results for 
Search instead for 
Did you mean: 

Using 2 USB OTG

arge
Associate III
Posted on December 03, 2013 at 14:48

Hello I want to use 2 usb otg peripheral units of stm32f205 MCU to transfer .wav files one to other.. Where can I find source codes from? Do you have any idea or suggestion? What problems do you think I have by using 2 usb? 

Thank you...

#2-usb-otg
1 REPLY 1
Posted on December 03, 2013 at 15:28

Well there's the USB firmware libraries, and the firmware update example in the STM32F4-Discovery examples (USB Flash + FatFs). There are perhaps some Olimex or eBay boards with two USB connections, you could see what they have. At the end of the day as a developer your likely to have to code your own solution.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..