cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with LWIP board fw in STM32f107

arge
Associate III
Posted on July 04, 2013 at 09:53

I have 2 devices with stm32f107 connected LAN. They are server mode and their fw is same except IP setting. I can connect each one by one at first time. But after I connected all when I try to connect  first I connected again it doesnt accept for a while.. After minutes i can connect..While i cant connect other ip client can connect too.

 What do you think about that? can it be a sw option, timeout etc. or is it about local modem? 

#problem-with-lwip-board-fw-in-st
4 REPLIES 4
Posted on July 04, 2013 at 13:13

What about the MAC addresses?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
arge
Associate III
Posted on July 11, 2013 at 11:13

definitely! you are right. I realized it after I wrote this discussion and it  is solved thank you..  

 i wonder how  is ETH_RMII_PPS_OUT  pin  usedit isnt used in STM example ethernet circuit with dp83848. PPS stands for pulse-per-second  right? What is the purpose of it ? 

 
Posted on July 11, 2013 at 11:52

Pulse Per Second.

In RM0008, look up ''PTP pulse-per-second output signal''.

JW
arge
Associate III
Posted on July 11, 2013 at 12:52

thx i already see in rm0008 but i want to see usage or example thank you .