cancel
Showing results for 
Search instead for 
Did you mean: 

L6234 Vref capacitor

marek23
Associate
Posted on April 04, 2013 at 20:26

The AN1088 app note states:

Vref ( Voltage Reference).

This is the internal 10V voltage reference pin to bias the logic and the low voltage circuitry of the device. A 1

m

F electrolytic capacitor connected from this pin to GND ensures the stability of the DMOS drive circuit. This pin can be externally loaded up to 5mA. Figure 3 and 4 show the typical behavior of the Vref pin.�

I was wondering whether a higher value ceramic capacitor can be used in place of the 1uF electrolytic capacitor on the Vref pin. For example, can we use a 4.7uF, 25V, ceramic, such as  C1608JB1E475K080AC? The app note does not describe whether there are other capacitor options.

Thanks!

#l6234-an1088
1 REPLY 1
Enrico Poli
ST Employee
Posted on April 10, 2013 at 17:21

The VREF capacitor can be ceramic, but its value should be >= of 1uF.

So the capacitor you indicated is OK.

Regards

Enrico