cancel
Showing results for 
Search instead for 
Did you mean: 

The question about the IEC60335's demo

aizhixi
Associate II
Posted on October 15, 2014 at 01:16

Now ,I use the  IEC60335_STM8Scome from ST,I encountered some problems.

I use the STM8S FOR IAR torebuilt the demo ,In a pity,i find that there are some error.

The MCU is STM8S903K3 ,theerror is unable to complete ''place at'' directives with a total estimated minimumsize of 0x800 bytes in <[0x000100-0x0007ff]> (total space 0x700).

I don't know why,i used theSTVD has the same condition。

                      That means the link file need to change ?right?

Can you help me ?

Tks so much.

0 REPLIES 0