cancel
Showing results for 
Search instead for 
Did you mean: 

Playback PCM audio file

rafael23
Associate II
Posted on May 13, 2013 at 11:19

Hi,

I am trying to playback a file with short PCM data recorded at 8KHz, 16bits, mono. I have tryed to configure the I2S with ''I2S_Standard_PCMShort'' but I can�t hear any sound. I have made a file like the file ''audio_sample.c'' included into the example, with the hexadecimal information of my PCM audio file.

Should I do something that I have missed? How should I configure the ''Interface Ctl 1'' registry of the audio codec? I have configured it like for the Phillips standard (0x04), but I don�t know if there is something different between both standards regarding this registry.

Thanks in advance.

#rtfm
5 REPLIES 5
Andrew Neil
Evangelist
Posted on May 13, 2013 at 14:27

''How should I configure the ''Interface Ctl 1'' registry of the audio codec?''

 

You must configure it in accordance with whatever the documentation for the particular CODEC tells you.

You haven't said what CODEC you're using - so it's impossible to be more precise!

Posted on May 13, 2013 at 15:01

Are you sure Mono is directly supported? I most case you have to map the sample to both channels.

Philips has ONE L
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rafael23
Associate II
Posted on May 14, 2013 at 12:56

Sorry, I forgot to say that my board uses a CS42L52 audio codec.

Finally I got it work using the Phillips standard, but with a very low quality of the sound and a lot of background noise. I have made test with a pcm file recorded at 48KHz (and of course played it back also at 48KHz), and the results are the same. I think that this problem is because of the ''mono'' configuration of the file as you have said. Can you guide me how to map the samples to both channels? Do you mean to write each sample twice to get the same sample in both channels?

Thanks for your help guys!

rafael23
Associate II
Posted on May 14, 2013 at 13:04

deleted

Posted on May 14, 2013 at 16:33

Can you guide me how to map the samples to both channels? Do you mean to write each sample twice to get the same sample in both channels?

Yes, basically.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Play%20mono%20on%20stereo%20channel&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=54]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FPlay%20mono%20on%20stereo%20channel&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=54
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..