2014-09-15 09:35 PM
Hello,
I'm trying to use STM32Cube to generate an IAR project from a 'Cube project configuration for the STM32F405. STM32Cube is installed, and will run, and will download the latest libraries. However when I press the ''generate source code based on user settings'' button, a box comes up with the message ''Generating user source code...'' and the program just hangs there. I've let it run for over an hour. The only way I can stop the program is to <ctrl><alt><del> and stop the process. When I do that a warning window pops up with the message ''The system cannot end this program because it is waiting for a response from you.'' However there is no such window open for me to respond to. Has someone else seen this problem and found a solution? Many thanks in advance, Geof #stm32cube-bug2014-09-17 09:06 PM
Well, I found a workaround...
Simply install Cube on a different computer, generate the project there, then send it back to the compute I want to use it on. Sneakers will never be obsolete. 🙂