cancel
Showing results for 
Search instead for 
Did you mean: 

ERROR REPORT - STM32H7x3 Reference manual : GPIO MODER

Julien FAUCHER
Associate III
Posted on March 23, 2018 at 22:30

Hi,

In the reference manual for the STM32H7x3 RM (RM0433) the register map for the GPIO in the GPIO register map (p.500) appear to be incorrect :

  • For the GPIOA, based on H7 Headers it's actually MODERx and not MODEx
  • For GPIOx : There is that 'MODEv1' bit which is also false (MODER).

Then, those three rows may be merged into one single row (excepted that the initial values aren't the same)

Best regards,

Julien FAUCHER♯

#stm32h7 #error #bug #documentation
1 REPLY 1
Nesrine M_O
Lead II
Posted on March 26, 2018 at 11:40

Hi

FAUCHER.Julien

,

Thank you for bringing these typos to our attention! It is noted and will be fixed in coming release of thedocument.

-Nesrine-