cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX feature request - Search for alternate pin functions

john doe
Lead
Posted on June 25, 2017 at 19:25

Currently the search in the pinout view searches the labels. It would be nice if there was some way to search pin functions, too. Eg., all the pins that have I2C2 anything as their alternate function.

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on January 29, 2018 at 17:30

Hi,

Ok for the search, it is only a pin search.

However, I fully agree with Imen, you have this function on the pin view.

Here is my example : 

I2C2_SCL is on H4-PH4 as below : 

0690X00000609XJQAY.png

and if you do a Ctrl Click, you have in blue the alternate functions (H3-PF1 and R12-PB10) : 

0690X00000609XSQAY.png

It is the way we decided to show the alternate functions.

BR. Jeanne

View solution in original post

11 REPLIES 11
Zt Liu
Senior III
Posted on June 26, 2017 at 03:30

I also need it too!

Let me add a pic for Jone, so that everyone can understand better!

(Following picture is extracted from FSL's(now NXP) KE Pin Tools.)

0690X00000602TsQAI.bmp
misagh
Associate III
Posted on June 26, 2017 at 10:36

Hi,

Actually there is an option: if you press ctrl key on keyboard and click on a pin, all alternates of this pin will change to blue. Also you can change the peripheral's pin by dragging the current pin to blue pin.

hope it would be helpful.

Bests,

Misagh

Posted on June 26, 2017 at 10:52

COOL!!

(I should read the following instruction first!)

0690X00000607TiQAI.png

Thx, Misagn!

Posted on June 26, 2017 at 11:24

Your welcome!

Posted on June 26, 2017 at 12:28

When I'm working with a bga216 chip I don't want to have to click on every ball to find a function, hence my request to add pin functions to the search.

Imen.D
ST Employee
Posted on June 27, 2017 at 16:17

Hi

doe.john.016

,

Please refer to the

http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM001047pdf/files/DM001047pdf/jcr:content/translations/en.DM001047pdf

STM32CubeMX User manual to have more insightabout

Manual Remapping

features.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on June 28, 2017 at 01:51

I'm talking about using the STM32CubeMX application to search for pin functions in stead of using the data sheet, that's all.  'find me all the pins with this alternate function.'

also it would be helpful if ST used a two digit pin  number because searching for PA01 does not give me pin 1 on port a. Searching for PA1 gives me all pins that being with PA1 including all the pins from pa11-pa19. When the labels are inconsistent, that means I have to click on up to 10 balls in order to find pin PA1. The search needs improvement.

Posted on June 28, 2017 at 10:27

Hi

doe.john.016

,

All your feedback are raised internally for further investigation.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on January 29, 2018 at 11:46

Hi

doe.john.016

,

I was reading this post and I am trying to reproducethe point you highlighted.

From the pin search, I am searching for PA1, I found it immediately in the combo box as below :

0690X00000609XDQAY.png

Is it what you need?

BR

Jeanne