2017-07-04 12:11 PM
uint32_t word0 = *(uint32_t *)(UID_BASE);
uint32_t word1 = *(uint32_t *)(UID_BASE + 0x04); // offsets taken from reference manual uint32_t word2 = *(uint32_t *)(UID_BASE + 0x08); uint64_t lotNum;bits 8:31 on word 1 are bits 23 through bit 0 of the batch number
word2 is bit 55 through bit 24 of the batch number
lotNum is the batch number, I think...
lotNum = ((uint64_t)word2 << 24 ) | (word1 >> 8);
2017-07-04 12:23 PM
also, the reference manual says word0 is X and Y coordinates. which is high and which is low?
Device Unique ID: 002B0036 33355111 36303934
Wafer 17 of Lot Q534906Location on wafer: X:54, Y:43len = 0;
char idString[128] = {0}; char lotNumString[32] = {0}; uint32_t word0 = *(uint32_t *)(UID_BASE); uint32_t word1 = *(uint32_t *)(UID_BASE + 0x04); // offsets as per reference manual uint32_t word2 = *(uint32_t *)(UID_BASE + 0x08); uint32_t x = word0 & 0xFFFF; uint32_t y = (word0 & 0xFFFF0000) >> 16; uint32_t wafer = word1 & 0xFF; uint64_t lotNum; lotNum = (((uint64_t)word2 << 24 ) & 0xFFFFFFFFFFFFFFFF) | ((word1 >> 😎 & 0xFFFFFFFF); len += sprintf(idString, 'Device Unique ID: '); len += sprintf(idString+len, '%08lX %08lX %08lX\r\n', word0, word1, word2); sprintf(lotNumString, '%s', (char *)&lotNum); // ASCII coded lot number len += sprintf(idString+len, 'Wafer %ld of Lot %s\r\n', wafer, lotNumString); len += sprintf(idString+len, 'Location on wafer: X:%ld, Y:%ld\r\n', x,y); printf('%s', idString);