cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Makefile Generator Reported Error while Updating Project

imi415
Associate II
Posted on June 07, 2018 at 18:44

After updating to CubeMX 4.26.0, Makefile projects cannot be updated due to the following errors:

0690X0000060BanQAE.png

2018-06-08 00:35:55,360 [INFO] ToolchainGenerator:120 - stack trace : java.lang.UnsupportedOperationException: Not supported yet.

at generators.MakefileGenerator.updateHeapAndStack(MakefileGenerator.java:315)

at generators.Generator.generateLinkerFile(Generator.java:715)

at generators.Generator.copyLinkerFile(Generator.java:407)

at convertor.Convertor.generateMakefile(Convertor.java:1436)

at convertor.Convertor.generate(Convertor.java:608)

at convertor.Convertor.convert(Convertor.java:515)

at convertor.Convertor.updateProject(Convertor.java:384)

at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.update(ToolchainGenerator.java:114)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1780)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:574)

at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)

#stm32cubemx.
1 ACCEPTED SOLUTION

Accepted Solutions
Nawres GHARBI
ST Employee
Posted on June 27, 2018 at 19:10

Hi All, 

There is an issue with regeneration of makefile project with the 4.26.0.

This will be fixed in the 4.26.1 which will be on the web soon

View solution in original post

11 REPLIES 11
Khouloud GARSI
Lead II
Posted on June 08, 2018 at 09:45

Hi

Sun.Sim

‌,

This is reported to our CubeMX team. One of our experts will answer you ASAP.

Khouloud.

Gavriil Pascalau
Associate
Posted on June 08, 2018 at 15:47

Hello,

I have the exact same problem when generating the Makefile.

Posted on June 08, 2018 at 15:59

Hi

gavriil.pascalau

‌,

This is already under check.

Thanks for your comprehension and sorry for such inconvenience.

Khouloud.

chaoyu chen
Associate II
Posted on June 15, 2018 at 10:36

I also encountered this problem! Please help to solve it. Was stuck here.

Nicolas Ducho0ud
Associate
Posted on June 18, 2018 at 12:01

Same problem since update to new cubemx 4.26.0

Nawres GHARBI
ST Employee
Posted on June 27, 2018 at 19:10

Hi All, 

There is an issue with regeneration of makefile project with the 4.26.0.

This will be fixed in the 4.26.1 which will be on the web soon

yuqlid
Associate

Today, I tried the 4.26.1.

but, this problem wasn't solved...

VPand
Associate

Hello,

I'm facing this issue with KeilProject and TrueStudioProjects also. Version 4.26.1. Problem is still not solved.

imi415
Associate II

However, after recent update to 4.26.1, project generator is completely unusable..

Code generation succeed while project generation always failing.

Updated system Java to 10 solved everything.

Makefile re-generation still fails.

Everything unstable now...