cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F412G-Discovery + StEmWin + SWIPELIST = HardFault

zhenya kravtsov
Associate II
Posted on December 19, 2016 at 08:55

The original post was too long to process during our migration. Please click on the attachment to read the original post.
3 REPLIES 3
adawang150
Associate II
Posted on December 19, 2016 at 09:48

I have carefully read this

http://www.kynix.com/uploadfiles/pdf8798/STM32F429ZGT6.pdf

 ,but I don't know what's the problem of your board.Sorry about that.
zhenya kravtsov
Associate II
Posted on December 19, 2016 at 10:08

The problem is not STM32F412G-Discovery. Problem StEmWin library. Demonstration code for this boardis written using StEmWin library. Everything works (more or less ..). But when I create a new module (window) using SWIPELIST there is a problem. As I understand it happens if SWIPELIST inherited from ICONVIEW (all your examples so made modules .. (windows) are inherited from ICONVIEW ). I think that a bug in the SWIPELIST because if it is not the error appears blank. Most likely a bug StEmWin library.. can you can somehow get around this problem? How can I use SWIPELIST using the demo code in which the parent is ICONVIEW? Question also asked on the forum SEGGER

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fmail.free-ide.com%2Findex.php%3Fpage%3DThread%26threadID%3D3744

but the answer did not get

:(

zhenya kravtsov
Associate II
Posted on December 20, 2016 at 07:13

Here is the link to the Russian forum 

http://forum.easyelectronics.ru/viewtopic.php?f=35&t=29792&p=478507#p478507